Symbol:
Function: This command repairs internal inconsistencies in the selected box.
Call: Main menu “FBD/LD/IL”, context menu
Requirements: The FBD or LD editor is active. The defective box is selected. The editor has found internal inconsistencies in the programming module that can possibly be resolved automatically. CODESYS reports the inconsistencies in the Message window.
This situation is conceivable when editing a project that was created with an older programming system version that did not yet handle the inconsistency concerned as an error.
See also