Symbol:
, shortcut: [Ctrl]+[Q]
Function: This command adds a further input to an extendable box (ADD, OR, ADD, MUL, SEL) above the selected input.
Call: “FBD/LD/IL” menu
Requirements: The FBD or LD editor is active. An input of a box is selected.
If a box is selected, the command “Append Input” is available in the context menu. The input is inserted at the lower end of the box.
See also