Symbol: 
Function: The command inserts an empty box with a Boolean input “Enable” and a Boolean output “Enable Out” at the end of the selected network.
Call: Main menu “FBD/LD/IL”, context menu
Requirements: The FBD editor, the IL editor or the LD editor is active. A network must be selected. No other box may be selected.
If “Enable” has the value FALSE at the time of the function block call, then the operations defined in the FB are
not executed. Otherwise, if “Enable” has the value TRUE, these operations are executed. The ENO output acts as a repeater of the EN input.
See also