Symbol:
Function: This command allows you to jump to any network.
Call: Main menu “FBD/LD/IL”
Requirements: The LD, FBD or IL editor is active. A network is selected.
This command opens a dialog box with an input field. Enter the number of the desired network in the input field.
See also