Function: This command is used for saving the library file to the hard disk.
Call: Context menu of the Library Manager
Requirement: A library is selected in the Library Manager.
The command opens the standard dialog for saving a file in the local file system.
The library file can have the file type Library files (*.library), Compiled library files (*.compiled-library), or Compiled library files (*.compiled-library-v3).