Symbol:
Function: This command exports all the text lists of the project.
Call: Main menu “Textlist”, context menu
Requirement
-
A text list or a global text list is open and active.
-
The visualization does not code the characters of the texts in Unicode.
CODESYS creates a file as plain text in the format .txt
for each text list. The name of the text list becomes the name of the file. The directory
into which the files are exported is set in “Project Project Settings Visualization”, category “General” in “Text list files”.
A controller can read and use this format. For example, you can copy the file to a controller and, by means of a configuration in the visualization manager, prevent the text lists from being transmitted again when loading the application.