Function: This command opens a dialog box for exporting objects from a project into an XML file in the PLCopen format.
Call: Menu “Project”
Dialog box 'Export PLCopenXML'
The dialog box lists all objects from the Device tree that CODESYS can export into an XML file in accordance with the PLCopen format.
The PLCopenXML scheme does not permit VAR_GLOBAL and VAR_GLOBAL CONSTANT POUs to be in the same variable list. Therefore, if you wish to export both, you must first divide the variables into two separate variable lists.
See also