Function: When multiple objects are available for an object, this command opens a dialog box for selecting an editor.
If only one editor is available for an object, then this command opens the object in that editor.
Call: Main menu “Project” or shortcut menu (right-click)
Requirement: An object is selected in the device tree or in the “POUs” view.
In the standard installation of CODESYS, there is no object that has multiple available editors.