Function: The command opens the dialog “Edit Declaration Header”, which serves in the declaration editor for the configuration of a POU header.
Call: Context menu of the tabular declaration editor
Requirements: The tabular declaration editor is the active editor.
Dialog 'Edit Declaration Header'
Function: The dialog is for configuring the declaration part of a POU.
Call: Click on the header bar of the tabular declaration editor, or context menu in the tabular declaration editor.
|
“Declaration” |
Selection list for changing the POU type
Input field with current POU name: you can change the name of the POU |
|
“Automatically adapt all references on rename” |
|
|
“Attributes” |
The dialog box “Attribute ” opens for the input of attributes and pragmas. |
: Dialog box
: Renaming is only effective in the declaration header of the POU.