Symbol:
Function: This command opens the “Document Project” dialog box, where you can define the project documentation. This includes the selection of objects in the open project that you want to print.
Call: Main menu “Project”
“Please select the objects which are to be printed” |
Project tree view In this view, you can select or clear objects for printing. All objects are selected by default. |
“Title page” |
CODESYS creates a title page named "Project Documentation" with the following information:
|
“Table of contents” |
CODESYS creates a table of contents for the project documentation. |
“Preview” |
CODESYS creates and opens a print preview of the project documentation. |
“Select” |
CODESYS opens a drop-down list of all or single object types for the project documentation. |
“Deselect” |
CODESYS opens a drop-down list of all or single object types that should be excluded from the project documentation. |
“OK” |
The “Print” dialog box opens. |