Function: This command switches back and forth between the enabled (activated) and disabled (deactivated) states of a device in the bus system.
Call: Context menu of a device object in the device tree.
Requirement: The project is in offline mode. The bus driver must support the function.
A disabled device is not taken into account and is not addressed. Note that with some bus systems the deactivation of a node can lead to the master stopping.
The entry of a disabled device in the tree appears in light-gray lettering.