Function: This command generates a boot application.
Call: Main menu “Online”.
A boot application is the application that is started automatically when the controller is switched on or started.
In offline mode, you can save the boot application in any directory. In online mode,
CODESYS save the boot application to the target device. The file name is <application name>.app.