Function: This command deletes the build information for all applications in the project.
Call: Main menu “Build”.
During the last download, the build information was created in the local file system and saved to a file (*.compileinfo).
This command requires a download before another login An online change is no longer possible. As compared to the “Clean” command (only the active application), CODESYS regenerates the language model for all objects, which is very time-consuming.




NOTICE

Reconsider carefully whether or not executing this command is really necessary. If you only want to rebuild and download the active application, then execute the “Clean” command.
See also