Symbol:  ; keyboard shortcut : [Ctrl]+[M] (to toggle between “S”, “R”, “REF”, and None)
; keyboard shortcut : [Ctrl]+[M] (to toggle between “S”, “R”, “REF”, and None)
Function: The command adds a Reset to the input of a Boolean “Output” element.
Call: Menu bar: “CFC Set/Reset”; context menu: “Set/Reset”
Requirement: A CFC editor is active. The input of an “Output” element is selected.
If an “Output” element has a Reset input, then the Boolean output value is set to “FALSE” as soon as the value of the input is “TRUE”. The “FALSE” value at the output is retained, even if the input value changes.
See also