Function: This command removes a control point.
Call: Context menu “Routing”
Requirements: A CFC editor is active. You have selected a connecting line.
If you move the mouse pointer over a selected connecting line, the existing control points are displayed with yellow circle symbols. Set the cursor on the control point to be deleted and execute the command from the context menu.
See also