This command is required when using compiler versions 3.5.11.x and 3.5.12.x. The command is no longer required for compiler versions >= 3.5.13.0.
Function: The command activates and deactivates the forceability of the inputs for a function block element.
Call:
-
CFC
-
Context menu
Requirements: The CFC editor is in offline mode and a function block element is selected.
After executing the command, the “Force Function Block Input” command is available in online mode to open a dialog for forcing the box input values.
See also
-
linktarget doesn't exist but @y.link.required='true'