Symbol:
Function: This command opens the “Breakpoints” view.
Call: Menu bar: “View”.
This view shows an overview of all defined breakpoints for an application. You have access to all breakpoint commands within this view.
|
“Application” |
Select the required application from the list. |
|
“POU” |
Name of the function block that will receive the breakpoint |
|
“Location” |
Location of the breakpoint in the POU
For function blocks, "(Impl)" indicates that the breakpoint is located in the implementation of the function block, not in an instance. |
|
“Instance Path” |
Complete object path of the breakpoint location. |
|
“Tasks” |
Names of tasks that will be effective when the breakpoint is executed. If there are no restrictions, then "(all)" is displayed here. |
|
“Condition” |
|
|
“Hit Count Condition” |
When the breakpoint should be in effect (depending on the hit count) |
|
“Current Hit Count” |
How often the breakpoint has already been reached up to now during the execution |
![]() |
|
This command opens the “Breakpoint Properties” dialog. |
|
|
This command opens the “New Breakpoint” dialog. |
|
![]() |
“Clear Breakpoint” |
Removes the breakpoint (not the same as disable) |
![]() |
“Enable/Disable Breakpoint” |
Toggles the status of the breakpoint or execution point between "enabled" and "disabled"
As opposed to "Clear breakpoint", a disabled breakpoint remains in the list and can be enabled again. |
![]() |
“Properties” |
The “Breakpoint Properties” dialog opens for editing the breakpoint parameters. This dialog is the same as “New Breakpoint”. In online mode, you can change the breakpoint into an execution point. |
![]() |
“Go to Source Position” |
Opens the online view of the affected block. The cursor is set at the breakpoint location. |
![]() |
“Clear All Breakpoints” |
Deletes all breakpoints and execution points in the application. The list is cleared. Not to be confused with "deactivate". |
![]() |
“Enable All Breakpoints” |
Enables all currently disabled breakpoints and execution points. |
![]() |
“Disable All Breakpoints” |
Disables all currently enabled breakpoints and execution points. The points remain in the list and can be enabled again. |





Breakpoint disabled
Execution point enabled
Execution point disabled
Data breakpoint disabled
Data execution point enabled
Data execution point disabled