Symbol: 
Function: This command opens the “Bookmarks” view.
Call: Menu bar: “View”.
|
|
Jumps to the bookmark that above the selected bookmark in the table and opens the respective POU in the editor. |
|
|
Jumps to the bookmark that below the selected bookmark in the table and opens the respective POU in the editor. |
|
|
Deletes the selected bookmark from the table and in the respective POU. |
|
List of bookmarks in the project with the following information: “Bookmark”, “Object”, and “Position”. You can edit the bookmark order per drag&drop. When you double-click a row, CODESYS opens the respective “Object” in the editor and jumps to this bookmark. |
|
|
“Bookmark” |
Name of the bookmark as assigned by CODESYS in ascending numerical order: “Bookmark_0”, “Bookmark_2” etc. If the bookmark is selected and you click in the field, then it is editable and you can modify the bookmark name. |
|
“Object” |
Name and project path of the POU where the bookmark is set Example: |
|
“Position” |
Position of the bookmark in the POU Example:
|