Symbol: 
Function: This command opens a submenu with objects that contain all objects that can be inserted, depending on the current position in the “Devices” or “POUs” view.
Call: “Project” menu, context menu in the “Devices” or “POUs” view.
Requirement: If CODESYS is to insert the object in the device tree, select an already existing object under which the new one is can be inserted indented. If CODESYS is to insert the object in the POUs tree, set the focus in any free place in the CODESYS window.