Function: This command opens the “Gateway” dialog where you can define a gateway channel and add it to the current device configuration.
Call: Menu bar: “Gateway” in the “Communication Settings” dialog of the device editor.
Dialog 'Gateway'
| “Name” | Name of the gateway. | 
| “Driver” | Driver type from a drop-down list. | 
| Driver-specific settings, for example: IP address, port | Editable after double-clicking the predefined value. A short description for each parameter is displayed in the lower part of the dialog. Note: You can also specify the address of a DNS domain. This has to begin with  | 
The dialog is also used for later editing of the gateway entries of your project.
See also