You can use the call stack for determining the current position of the program flow. This function is very useful when stepping into programs.
Requirement: The application is in online mode. The program is halted at a breakpoint or you are stepping into it.
-
Open the call stack by clicking “View Call Stack”.
The call stack opens. The list shows the current location with the complete call path.
The call stack is also available in offline mode and normal online mode (without using debugging functions). In this case, it receives the last displayed location during a stepped execution, but it is displayed in gray.