|
“Node-ID” |
The node number identifies the CANopen Manager as unique (range of values: 1...127). |
|
“Check and Fix Configuration” |
Opens the dialog of the same name. See below for details. |
|
“Autostart CANopen Manager” |
Hint: As long as the CANopen Manager is not in OPERATIONAL mode, no PDOs are sent (outputs refreshed). |
|
“Polling of optional slaves” |
Constantly polling the slave increases the bus cycle time, which can interfere with the application (especially motion applications). You can deactivate polling to avoid this behavior. If polling is deactivated, then a slave is detected again when it sends a bootup message. |
|
“Start slaves” |
|
|
“NMT start all (if possible)” |
|
|
“NMT error behavior” |
|
|
Working with heartbeat messages is an alternative method of monitoring. It can be executed from both master and slave nodes, as opposed to node guarding. Normally the master sends heartbeat messages to the slaves. |
|
|
“Enable heartbeat producing” |
The master sends heartbeats. They define the time interval in the “Producer time”. When the slaves are provided with the heartbeat function, a heartbeat consuming entry from the slave is created for the master. Then the Node-ID and the 1.5x heartbeat interval of the master are applied.
|
|
“Node-ID” |
Unique identification (1-127) of the heartbeat producer on the bus |
|
“Producer time (ms)” |
Interval length between successive heartbeats (in milliseconds) |
|
“Redundancy Node-ID” |
Requirement: A “Redundancy Configuration” object is inserted below the application. Unique identification (1-127) of the redundant heartbeat producer on the bus |
|
“Redundancy wait time (µs)” |
Requirement: A “Redundancy Configuration” object is inserted below the application. Duration of how long the passive controller waits for the heartbeat of the active controller. If this time is exceeded, then the passive controller takes on the active role. |
|
“Enable SYNC producing” |
The synchronous PDOs are sent directly after the SYNC telegram. |
|
“COB-ID (Hex)” |
CAN-ID of the SYNC telegram. Range of possible values: [1...2047]. |
|
“Cycle period (µs)” |
Interval length (in microseconds) after which the SYNC telegram is sent |
|
“Window length (µs)” |
Length of the time frame for synchronous PDOs (in microseconds) |
|
“Enable SYNC consuming” |
|




NOTICE

If SYNC producing is enabled for the CANopen manager, then you are not permitted to select the “Enable SYNC producing” option for all other bus devices.
|
“Enable TIME producing” |
|
|
“COB-ID (Hex)” |
(Communication Object Identifier): identifies the time stamp of the message. Default values: [0...2047], preset 16#100 |
|
“Producer time (ms)”: |
Interval (in milliseconds) when the time stamp is sent. This value has to be a multiple of the task cycle time. Possible values [0, 65535] |
The run time has to support high resolution timestamps. If not, then an error message is displayed.
Dialog 'Check and Fix Configuration'
If you insert several devices below the CANopen manager, then error messages may report multiple assigned Node-IDs or invalid COB-IDs. The “Check and Fix Configuration” button opens a dialog for solving these conflicts.
For conflicts with Node-IDs or PDO COB-IDs, you can click “Edit Conflicts” to open a dialog with detailed information.
|
“Doubled node number” |
List of all devices with identical IDs. In the field of the “Node-ID” column, you can enter new node numbers for the affected devices. |
|
“Incorrect and double assignment of PDO COB-IDs” |
The COB-IDs that are generated automatically from the device description files may not be permitted. All incorrect entries are listed with the respective device names, Node-IDs, and indexes. There are three options for correcting invalid COB-IDs:
|
Corrected entries are removed from the displayed list automatically.
You can solve timing problems automatically by using the “Automatic Repair”. The command modifies all timing values to compatible values. (The time should be a multiple of the task time.)
: The CANopen Manager starts automatically (switches to OPERATIONAL mode) after all
required slaves are ready.
: The CANopen Manager has to be started from the application. The function block